FB#.HALLMAP.V

Description

FB#.HALLMAP.V reads and writes to a mapping register used to correct mis-wired motors without physically changing the wiring. This keyword only effects feedback devices that have halls (see FB#.SELECT for feedback types with halls).

FB#. HALLMAP.V can be set to one of the following values:

Value

Description

0

The output is the U input value. (Swap V with U)

1

The output is the V input value. (Default)

2

The output is the W input value. (Swap V with W)

3

The output is fixed at 0.

4

The output is U input inverted value. (When input U=0, V output is 1)

5

The output is V input inverted value. (When input V=0, V output is 1)

6

The output is W input inverted value. (When input W=0, V output is 1)

7

The output is fixed at 1.

Versions

Action Version Notes
Implemented 02-10-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 7

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.HALLMAP.V

3500h

1ch

Unsigned8

-

-

Read/Write

No

FB2.HALLMAP.V

3501h

1ch

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30760

1

30760 (0x7828)

FB1.HALLMAP.V

Unsigned8

Read/Write

Yes

30761

1

30761 (0x7829)

FB2.HALLMAP.V

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.HALLMAP.V

30760

Unsigned8

Read/Write

-

FB2.HALLMAP.V

30761

Unsigned8

Read/Write

-

Related Topics

FB#.HALLSTATE

FB#.HALLMAP.U

FB#.HALLMAP.W

FB#.SELECT